Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: IWR6843, IWR6843AOP, MMWAVEICBOOST
Hi,
I programmed IWR6843AOPEVM Revision G for a people counting application and it works with UARTs over USB and I can visualize the data. I was trying to get the same data over BLE and I set the switch configuration based on the EVM user guide. I have connected to the Bluetooth module named "Simple Peripheral" using the passcode "123456" and now I have two COM ports called Standard Serial over Bluetooth link. But, I can not get any data from them. Is there any extra programming or config that should be done?