What the external connections are needed to connect the IWRL6432 chip with MCU? (like XTAL)
Which MCU are you using for IWRL6432 application?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What the external connections are needed to connect the IWRL6432 chip with MCU? (like XTAL)
Which MCU are you using for IWRL6432 application?
Hi Gayathri,
Please refer to the IWRL6432 product page and the IWRL6432BOOST product page, on which you can gain the information you are looking for in the schematic. Specifically, I would reference the schematic for the IWRL6432BOOST EVM, which will show how an XTAL is connected to the device.
For example, this functional block diagram comes from the product page, in which you can see that we use an ARM Cortex M4F core:
Regards,
Luke