Other Parts Discussed in Thread: DCA1000EVM, AWR1642BOOST, IWRL6432
Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
"I am starting to use the mmWave module IWRL6432BOOST and I'd like to know more about the configuration file parameters and how to set those. The device isn't supported in the Sensing Estimator like with other TI mmWave devices so it is difficult to figure out exactly how to set the chirp parameters and optimize them for my use case.
I sadly do not have access to a DCA1000EVM as they have been out of stock for a long time while I've had this device so I would like to see if I can communicate with it via serial and not have to rely on the data capture board.
The mmWave SDK manual was very helpful in figuring out the components but I can't seem to get the board to work with the Demo Visualizer.
It works with an AWR1642BOOST module which is running on SDK 2.0, but when I set it to 3.x, it is not able to connect to the 6432 board, despite me using the correct UART and Data com ports via USB. Is there any way you could help me resolve that? I have the on-board switches set to functional mode (S1.1 is on).
The error describes itself as the status in the bottom info bar on the Demo Visualizer showing it has managed to connect to one of the COM ports, but is failing to connect to the second and it keeps looping around there without showing any other signs of errors or fault.
Please help to advise. Thank you for extending your support.
Kind regards,
Marvin