This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Error transferring files using Winscp

Part Number: AWR2243

/mnt/ssd/Cascasde_0529_00/  This is the SD  data.  The data size of master and slave1 is both 29184KB

MmwaveStudio error:

Why transfer this file:“remove_0000_data.bin"

And the transferred file is:

An additional file has been added,”remove_0000_data.bin“

Two files are missing:”master_0000_idx.bin“ and "slave1_0000_idx_bin"

The size of file "master_0000_data.bin" and "slave1_0000_data.bin" are not correct.

I tried restarting Mmwave Studio and running ”Cascade_ Configuration_ MIMO.lua“ and ”Cascade_ Capture.lua“ file and uninstalled and reinstalled the “winscp” software, but this does not solve this problem. May I ask how to handle this issue?

Thank you  very much!