Other Parts Discussed in Thread: IWR6843ISK
Hello,
I have purchased IWR6843ISK and IWR6843ISK-ODS before.
I tried to play with those two modules using also DCA1000 board to extract raw data.
In briefly summary, when I have utilized 'mmWave Studio' and 'mmWave Demo Visualizer' programs,
I commonly found that IWR6843ISK operates well, but IWR6843ISK-ODS does not work whether DCA1000 board is connected or not.
For example of using IWR6843ISK-ODS,
in 'Connection' tab with 'mmWave Studio' (I am sorry, I cannot upload any figure due to the company's security issue)
'No.of Devices Detected' : 0
'FTDI Connectivity Status' : connected
'RS232 Connectivity Status' : Disconnected
'SPI Connectivity Status' : Disconnected
and, BSS FW cannot be loaded.
Also, four COM PORTs for 'AR-DEvPack-EVM-012' is not assigned in Device Manager in this case.
On the other hand, IWR6843ISK is working very well without device recognition failure.
For more explanation in the case of using 'mmWave Demo Visualizer' program,
I found the messege, "connecting to 1 of 2 targets" for 'ISK-ODS' (from checking the connection status in the bottom of the progam tab.) even though two COM ports are assigned in 'Device manager' in PC. On the other hands, when I use 'ISK' in the same way, "connecting to 2 of 2 targets" is found and radar operates successfully.
So I guess something is wrong in IWR6843ISK-ODS antenna module itself.
Please let us know some solutions with the point of view for antenna module itself.
If it is needed, there seems a serial number backside of each antenna board (ISK : 6382600161, ISK-ODS : 6383100218).
Thanks.
B.R.,
Junseuk.