This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP441: DUT integrated ESD diodes as thermal diode

Part Number: TMP441

Hello Sensors Team,

Would it be possible to use the TMP441 together with a Device Under Test integraded ESD diodes (i.e. ESD diode integrated at GPIO pin to Vdd and Vss) to perform temperature measurements on the DUT? The DUT is a IC without internal thermal diodes.

In case TMP441 cannot be used for such a use case, is there an alternative TI part which can support this?

Regards,

Viktor