Other Parts Discussed in Thread: IWR6843ISK
Hi experts.
We are developing out project based on the example code of presence_motion_detect.
And the config parameter which satisfied our test scene is generated by adjusting parameter by the mmWave Sensing Estimator page linked as following:
https://dev.ti.com/gallery/view/mmwave/mmWaveSensingEstimator/ver/2.2.2/
then we got 50 Frame Periodicity while set Measurement Rate to 20.


However set Frame Periodicity to 50 seems not works at all.
By referring to the similar issue as following link:
The valid range of FramePeriodicity is shown between 100 to 4294967295 that means maximum frame rate is restricted to 10 Hz in IWRL6432.
We are curious about that is FramePeriodicity the only one parameter can change frame rate?
If not so, is there any other method to adjust frame rate?
Thanks.
Regards.