The title says it all. I am using TI CCS v 12 and am trying to pass CLI commands into the MMWave Demo during debug. I flashed the xwr6843_ccs_debug image onto the board, build the mmwave demo project in TI CCS, and then entered debug mode. However, I need to pass CLI commands to start the sensor.
Is there a way to do this using TI CCS? Or do I have to hardcode the configuration for this scenario?