HI SIR
Due to HTU21D is out of stock, my I know the TI /hdc2080 Can replace it direct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI SIR
Due to HTU21D is out of stock, my I know the TI /hdc2080 Can replace it direct?
Hello Chen,
The devices are mostly pin to pin from a hardware stance. Note that the HDC2080 also includes an ADDR pin(pin 3), which must be tied high or low and also DRDY/INT, which could be ignored if you don't need to use this pin.


From an interface/software stance, the devices are not compatible and the software would need to be implemented for HDC2080. You can find MCU agnostic code examples and configurations below.