Other Parts Discussed in Thread: IWR1843,
Hi
I have some questions about HWA 2.0.
1) Where is HWA 2.0 user guide?
I confirmed that there is HWA 1.0 user guide for IWR1843.
2) Is it possible to use HWA for applications other than FFT, CFAR and log magnitude?
For example, Is it possible to use the HWA to execute a custom complex multiplication operation?
3) Is input data for HWA 2.0 complex number only?
For example, When I input Real number for HWA, should the Q sample be zero?
Regards,
Naoya