Hello,
The TMP468 datasheet states that the assigned address depends on the ADD pin, but it does not specify when the ADD pin is actually read/strobed to determine address.
During which state is the ADD pin read to determine address?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The TMP468 datasheet states that the assigned address depends on the ADD pin, but it does not specify when the ADD pin is actually read/strobed to determine address.
During which state is the ADD pin read to determine address?
Thank you
Hello Roy,
The ADD pin is sampled at the address phase of every I2C transaction. Let me know if there are other questions.