This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: AWR1642 EVM RF power Spectrum Analyzer Anomalies

Part Number: AWR1642

Our company encountered a strange phenomenon in the application of AWR1642. At the frequency point of 78.4GHz, the RF POWER will appear as shown in the screenshot below, and the phenomenon will drop by 2.5dBm in an instant. It has been confirmed that the EVM also has such a phenomenon.

I checked the document of AWR1642 DeviceSilicon Errata, and there is no description of this problem. Can you help to clarify whether it is a problem with the software setting or the chip itself?

  • Hello Jeff,

    Can you share the profile configuration and chirp configuration you are using?

    Regards,

    vivek

  • sensorStop
    flushCfg
    dfeDataOutputMode 1
    channelCfg 15 5 0
    adcCfg 2 1
    adcbufCfg -1 0 1 1 1
    profileCfg 0 77 429 7 57.14 0 0 70 1 256 5209 0 0 30
    chirpCfg 0 0 0 0 0 0 0 1
    chirpCfg 1 1 0 0 0 0 0 4
    frameCfg 0 1 16 0 100 1 0
    lowPower 0 0
    guiMonitor -1 1 1 0 0 0 0
    cfarCfg -1 0 2 8 4 3 0 15 1
    cfarCfg -1 1 0 4 2 3 1 15 1
    multiObjBeamForming -1 1 0.5
    clutterRemoval -1 0
    calibDcRangeSig -1 0 -5 8 256
    extendedMaxVelocity -1 0
    lvdsStreamCfg -1 0 0 0
    compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
    measureRangeBiasAndRxChanPhase 0 1.5 0.2
    CQRxSatMonitor 0 3 5 121 0
    CQSigImgMonitor 0 127 4
    analogMonitor 0 0
    aoaFovCfg -1 -90 90 -90 90
    cfarFovCfg -1 0 0 8.92
    cfarFovCfg -1 1 -1 1.00
    calibData 0 0 0
    sensorStart

  • Hello,

    What is the measurement setup you are using? Do you have down converter to bring the RF frequency to a lower value? If yes can you check if this artifact is caused due to the down converter? If you slightly shift the external mixer clk input frequency and the point at which this step power reduction occurs also shifts, then it will help separate out the point at which this issue is occurring.

    regards,
    vievk

  • Thanks to Vivek for his assistance