Other Parts Discussed in Thread: IWRL6432
I'm able to run the application from the CCS debugger successfully. But when I flash the appimage to the board using low power visualizer provided in the SDK, the program doesn't run as expected (we were able to know, because the config is sent from CLI, but it doesn't get past the first command from the config file). In the debugger after loading the program, we load a binary file from the SDK at a memory address as explained in the CCS debug guide of IWRL6432, from my understanding that binary file is not part of the appimage, so we are getting errors. The appimage is built with both debug and release build targets and the SDK version is MMWAVE_L_SDK_05_02_00_02.