This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Is it possible To change two parameters at the same time in Advance Chirp

Part Number: AWR2243


Hi,All.

Is it possible to change  StartFreq and Idle Time at the same time in Advance_chirp?

for Example,

1st chirp : StaretFreq is 76GHz, IDle Time is 10us

2nd chirp : StaretFreq is 76GHz+10MHz, IDle Time is 10us+0.2us 

3rd chirp : StaretFreq is 76GHz+20MHz, IDle Time is 10us+0.4us 

512th chirp : 2nd chirp : StaretFreq is 76GHz+10MHz*511, IDle Time is 10us+0.2us*511

Thanks.