Executing the demo as instructed goes well until the very last step.
When pressing resume, the console reads as follows and does not progress further than that until I either disconnect or manually stop the demo, but still the console remains unchanged.
- [Cortex_M4_0] Calibration Validated for restore
The switches on the device are as follows and are copied directly from both the image in the document and the description on the same page:
S1: 110010
S4: 0001
I am unable to communicate with the device over UART via the USB link included and a super simple python script using the Serial package but running all Visualizer demos works as intended.