This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
not software, updated hardware or a new item/ similar item that can control PWM of at least 2 devices simultaneously.
The LM96000, LM93, LM94 and LM96194 all have at least 2 PWM channels. None of these legacy devices have an EVM.
thanks,
ren
Ren,
I need a PWM controller that i can plug a DC fan into and control through a GUI on my PC and is compatible with windows 10..... it should be able to control at least two fans independently and simultaneously. I do not need temperature readings or anything else. i just need 4 pins, gnd, pwr, tach, and pwm that is pluggable (meaning no soldering required like the EVM).. I do not need an a IPD or the LM-line of components. There are a lot of devices available on the market that can do this, i wanted to know what TI's latest product in this category is. If it does not have one, then I will look elsewhere. Please advise. Thanks
Okay. It was a good product, wish TI continued support/ updates.
Thanks for your time, Ren. Appreciate the support.