Hello TI,
I'm working with the FDC2214 right now and trying to understand how the current driver works. Referencing this post: https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/852838/fdc2214-current-drive-control-registers I had the following questions:
- Is there an updated datasheet for the FDC2214? The aforementioned post mentioned an error in the datasheet and going to fix it in the next revision.
- What is the INIT_DRIVE current field? There doesn't seem to be any register with that field.
- In full current drive mode, does the 2214 drive with the max current, then settle to the minimum current required to have a Vpk between 1.2V to 1.8V? If so, does that essentially automatically set the timing of the system?
Thanks!
Eugene