This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: CASO-CFAR low range resolution (FCC compliant) mode in overhead mode (build configuration)

Part Number: IWR6843AOP


Hi,

The radar_toolbox_1_10_00_13\source\ti\examples\People_Tracking\Overhead_3D_People_Tracking\ laboratory support a build configuration intended to be used for chirp configuration with less than 500 MHz of bandwidth and maximum transmitter power. This build configuration affects the CFAR-CASO implementation through the #define  CFAR_LOW_BW (RADARDEMO_detectionCFAR_raCAAll() in \dpu\capon3d\modules\detection\CFAR\src\RADARDEMO_detectionCFAR_priv.c)

It is not clear to us if this build configuration shall be applied also to the wall-mount processing chain of the laboratory \radar_toolbox_1_10_00_13\source\ti\examples\People_Tracking\3D_People_Tracking in case we using a low bandwidth configuration (less than 500 MHz BW and maximum power) with a wall-mount setup. In particular, the build configuration for the low bandwidth CFAR is needed for the wall-mount processing chain?

Another question: the HWA support this CFAR LOW BW algorithm implementation?

Best Regards,

Riccardo Repetto