This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: Ability to distinguish between two or more objects.

Part Number: AWR1443BOOST

Hello,

I wanted to ask you that, how far must two objects be from each other for the radar to evaluate/distinguish them as two and not as one?

Is it dependent on the distance from the radar?

(In mmWave Demo Visualizer is Range resolution set on 0,044 m, but I think it is more than that in real)

Thank you

Best wishes, Robert