Hi,
My question is quite simple, do you recommend to add ferrite bead between the electrochemical cell pins and the LMP91000 ?
I've done a research on the net and I didn't find anything about that. There are some applications notes that recommend to do it but it's for other analog front end.
My question is because we have some EMI issue with our design which is based on the LMP91000 + ferrite beads.
I had the opportunity to do some house test with a homemade BCI and I noticed the LMP91000 output is more disturbed with the ferrite beads than without.
I'm wondering if it's better to check another ferrite bead reference or to remove them ?
Thanks in advance for your help
Nicolas