Hello,
I am creating a range doppler map from the raw data samples acquired using DCA1000 and AWR1843BOOST. I am checking the range doppler map moving my hand towards and away from the radar. The motion seems correct but I do not fully understand why the doppler values (velocity) appears mirrored across the zero axis. That means, when I see a blob moving near the center of the plot i also see a similar blob moving in the bottom or upper part of the plot? I am just running an FFT on both fast and slow time to compute this range doppler map.
See in the attached image there are simmetrical areas near the center.