Other Parts Discussed in Thread: AWR1642
Hello,
I've 2 questions please ,
1) how can I add watchdog functionality to my project on DSS on AWR294x ?
2) in the datasheet
Timers and Watchdog Module
– Five Real Time Interrupts (RTI) modules, three in MSS and two in DSS.
– Two Watchdog modules, one in DSS and one in MSS (Same RTI IP but in Watchdog configuration)
15.1.1 Features
The RTI module has the following features:
• Two independent 64 bit counter blocks
• Windowed Watchdog Timer (WWDT) Feature
• Four configurable compares for generating operating system ticks or DMA requests. Each event can be
driven by either counter block 0 or counter block 1.
• Fast enabling/disabling of events
• Two time stamp (capture) functions for system or peripheral interrupts, one for each counter block
• Digital windowed watchdog
Is there 2 types of watchdogs ( digital and not digital) ?