This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: TX transmitting power for different central frequency from 77GHz to 81GHz with 1 GHz bandwidth

Part Number: AWR1843

No matter of design of antenna (Skip the antenna S11 design issue for this question)

Settings:

SOC: AWR1843 (3Tx 4Rx)

Backoff: 0

RX gain: 48

Will the different central frequency (1GHz bandwidth) impact the TX transmit power?

For example: 

* Chirp 1: 76GHz ~ 77GHz (Central freq. 76.5GHz)

* Chirp 2: 77GHz ~ 78GHz (Central freq. 77.5GHz)

* Chirp 3: 78GHz ~ 79GHz (Central freq. 78.5GHz)

* Chirp 4: 79GHz ~ 80GHz (Central freq. 79.5GHz)

* Chirp 5: 80GHz ~ 81GHz (Central freq. 80.5GHz)

 

Antenna design issue aside, will the TX transmit power differ for Chirp 1/2/3/4/5?

Thanks.