I'm designing a board that uses the IWR1642, but there's some confusion on what the actual SOP pins are on the device. On page 2 of the "Bootloader Flow" application note (SWRA563), it lists the SOP pins as P13, P11, and J13 for SOP[2], SOP[1], and SOP[0] respectively. In the actual datasheet for the device (SWRS212B), the SOP pins are listed as P9, G13, and N13. I'm assuming that the datasheet is the correct one, but I wanted to verify before I put anything to copper. I couldn't find a schematic for the IWR1642BOOST EVM board, otherwise I would have just used that to verify.