Other Parts Discussed in Thread: AWR1843BOOST, AWR1843, AWR2944
Hello,
We are currently working on AWR1843AOP for one of the ADAS application. We have a desired detection range of 100m and above and by changing the initial configuration parameters, we have been able to achieve max range of 40m for a two-wheeler bike. We also used the TI sensing estimator to find out the desired configuration to achieve 100 m range and found out following configuration that is desirable for more than 90m. However, when we use the configuration, we are unable to receive the detections. Can you check on it once?
Following are the details of chirp and frame configurations
% with mmWaveBasic SDK without calibrating digital processing chain.
% ===============================================================================
profileCfg 0 77 2 5 21.26 0 0 9.75 1 62 4064 0 0 30
channelCfg 15 7 0
adcbufCfg -1 0 1 1 1
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 0 0 0 0 0 4
frameCfg 0 2 334 0 40 1 0
We had chosen AWR1843 AOP to focus more on the SW design rather than the RF design due to the limited competence on the RF design, If if AWR1843AOP is limited to a range detection <100m, then we'll have to go with other TI radar solutions. In that case, can you suggest the alternatives to AWR1843AOP in the frequency band of 77-81GHz? Also, Is there a reference document on designing our solution AWR1843BOOST with patch antenna just like the one available on EVM board?