Other Parts Discussed in Thread: AWR6843
When I send the config b"guiMonitor -1 1 1 0 0 0 1\n' to chip using the UART command port, i meet this issue, the reponse is 'guiMonitor is not recognized as a CLI command', but other commands can be set successfully, I want to know if this command is supported on IWR6843LEVM?
By the way, i want to get the output data using UART data port (baudrate is 921600)? how can i control the output data format?