Hey,
We designed a custom variant of a ti dlp reference board (TMP411-Q1) to readout the build-in temp sensor in the DLP.
At the moment we are using the TI light crafter gui to control and read out the sensor values of the ti board and also our board.
We can only readout the internal temperature sensor of the TMP411 correct.
For the external temperature it looks like that there is a offset.
After powerup of the board we get always 0°C back and after some operation time (the dlp warms up, not measured yet but would guess DLP temp is >30°C) the external temperature readout also increase.
W checked the schematic of our board many time and didn't see any issue there.
We also have the same circuit for a different board where it works quite well.
Have you an idea what can lead to such a behavior?
Many thanks
Best Christoph