Hi team,
"GAIN_VALUE" says that "The gain value is anywhere between 0 and 2. Gain is calculated as 'user entered value/1024" shiown in "Table 7-23. MAG_GAIN_CONFIG Register Field Descriptions." However, "8.2.2 Detailed Design Procedure" shows "The gain adjustment value is a fractional decimal number between 0 and 1." Which is correct one?
For example, considering that Bx gain is configured twice as By gain, then do we set "GAIN_SELECTION" as "2h" and "GAIN_VALUE" as "0h", is it correct?
Regards,
Ochi