Hi, supporter,
In the TDC7201 datasheet, section 7.3.3.3 "Clock Counter STOP Mask" mentions that setting TDCx_CLOCK_CNTR_STOP_MASK_H and TDCx_CLOCK_CNTR_STOP_MASK_L determines the mask window's size, and the STOP signals within this mask window will be ignored.
Based on my understanding, the mask window should only affect the Clock values in Mode 2 (TDCx_CLOCK_COUNT1 to TDCx_CLOCK_COUNT5). However, when I use Mode 1 measurement mode and set TDCx_CLOCK_CNTR_STOP_MASK_H and TDCx_CLOCK_CNTR_STOP_MASK_L, it seems to impact the Time clock values as well (TDCx_TIME1 to TDCx_TIME6).
Could you please confirm if this behavior is correct?