This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: mmWave Studio Cli application's configuration issue

Part Number: IWR6843ISK
Other Parts Discussed in Thread: MMWAVEICBOOST,

Hello TI experts,

 

I have a problem configuring IWR6843ISK + MMWAVEICBOOST which is flashed as mmwave studio cli.

I sent below commands to the device through Tera Term. Commands were seemed to work well but profileCfg command did not work and I kept receiving an error -51 (guide tells me that -51 means wrong number input). 

Can anyone help me what number I should input for command 'profileCfg' when I use mmwave studio cli?

It would be great if you give an example of this command.

 

Here is the Cfg commands that I tried to input for modulation.

sensorStop
flushCfg
dfeDataOutputMode 2
channelCfg 4 3 0
adcCfg 2 1
profileCfg 0 60 138.24 5.38 135.81 0 0 0 0 0 0 7.821 38.45 256 2000 0 131072 30
chirpCfg 0 0 0 0 0 0 0 1 1 1
frameCfg 0 0 0 32 10 0 0 1
sensorStop

 

Thank you.