Hello Guys
I built my circuit based on 6843AOPEVM(The pin configuration is identical to the 6843AOP with unused components removed.)
Due to the size of the board, I made a 10Pin JTAG configuration based on the link below.
software-dl.ti.com/.../emu_jtag_connectors.html
The circuit configuration is as follows. For the 10-pin header of XDS110, the header provided at the time of purchase was used.
As a result of JTAG Test Connection using CCS, the following error occurs.
I've never made progress by changing the JTAG configuration, so it's hard to pinpoint the problem.
I have a hard time analyzing the problem. I need help.