Other Parts Discussed in Thread: AWR1843AOP, AWR1843BOOST, AWR1843
Hi,
Now I test the AWR1843AOPEVM with the same bin file 18xx_mss_demo.bin, if the object is on the left lane, if I use the AWR1843BOOST, the azimuth is plus,but if the AWR1843AOP EVM is used, the azimuth is minus.
They have opposite signs.Is that right? If it is right, what is the reason for that?Is it with the Rx antenna layout?
For AWR1843BOOST, the antenna layout is as belows:
For the AWR1843AOP,the antenna layout is:
The Rx antennas sequence from left to right for the AWR1843Boost is RX1,Rx2,Rx3,Rx4; but for the AWR1843AOP is Rx4,Rx3,Rx2,Rx1, is it the reason for that?
Thanks,
Rata