I use AWR1843Boost with lab demo mrr.
In the demo, the CAN bus rate are configured 1Mbps and 5Mbps as nominal and data bit rate respectively.
I have configured the bus trate 500Kbps and 2Mbps as nominal an data bit rate successfully.
/*500Kbps NomBitRate: (40)/(((6+5+4)+1)*5)*/
mcanBitTimingParams.nomBrp = 0x5U;
mcanBitTimingParams.nomPropSeg = 0x6U;
mcanBitTimingParams.nomPseg1 = 0x5U;
mcanBitTimingParams.nomPseg2 = 0x4U;
mcanBitTimingParams.nomSjw = 0x1U;
//2 Mbps
mcanBitTimingParams.dataBrp = 0x4U;
mcanBitTimingParams.dataPropSeg = 01U;
mcanBitTimingParams.dataPseg1 = 0x2U;
mcanBitTimingParams.dataPseg2 = 0x1U;
mcanBitTimingParams.dataSjw = 0x1U;
But I could not successfully configure the data bit rate to 500Kbps. Can you advice how to configure data bit rate to 500Kbps?
Thanks