Hi,
In the 'mmwave_automotive_toolbox_3_6_0',the configuration is "frameCfg 0 5 128 0 384 250 1 0",but in the 'radar_toolbox_1_10_00_13' that is "frameCfg 0 5 128 0 384 50 1 0".The frame length is reduced to 50ms from 250ms. And how did you do it? Does it mean that one frame data can be processed in 50ms?
BR,
Rata