Other Parts Discussed in Thread: IWR6843, , MMWAVEICBOOST
Hello Expert,
Could you please write your comment at each items after checking my inquiries?
1. Is the UART Port (V16, U16) usable for program download in program mode and for external communication in operation mode?
2. Which pin can we use for RS-232 communication?
3. Is IWR6843 capable of RS-485 communication?
4. Do I need to use an external EEPROM (U6/CAT2408)?
5. Can I understand SOP CONFIGURATION mode as follows?
-. Functional Mode: Product operation mode
-. Flash Mode : Program download mode
-. MMWAVEICEBOOST mode: program download debug mode using JTAG
6. In the IWR6843AOP Data sheet, GND has VSSA and VSS separately, but GND is integrated in the EV circuit. Can it be integrated and designed?
7. I need Hardware Design Checklist for this part.
Best Regards,
Michael