What is the maximum angle error X-Y axes In temperature range -40 : 85degC? In datasheet it is only typical value

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the maximum angle error X-Y axes In temperature range -40 : 85degC? In datasheet it is only typical value

Hi Mateusz,
Thanks for posting to the Sensors forum.
Total angle error is system and test-condition dependent. These typical values are at 25°C with specific RANGE (10) and CONV_AVG (101b) settings.
As noted in the datasheet in section 9.1.5 Error Calculation During Angular Measurement, relevant error sources during angular measurement include sensitivity error, offset, noise, axis-axis mismatch, nonlinearity, drift across temperature, drift across lifetime, and so forth. The Angle Error Calculation Tool is provided to estimate total error during angle measurement.
Best regards,
Jesse