Part Number: IWRL6432BOOST
Other Parts Discussed in Thread: UNIFLASH
I'm currently trying to use the Industrial Visualizer with the IWRL6432BOOST board to run the Presence and Motion Detection demo, but Uniflash continues to flag an error when trying to load the image onto the board. I get the following error every time:
Error!
Cannot read System Setup data from XML file C:\Users\deyleb\AppData\Local\Temp\ti_cloud_storage\uniflash_temp.ccxml Error parsing file: Fatal Error at (25, 46): An exception occurred! Type:UnexpectedEOFException, Message:The end of input was not expected
I should have the correct COM port selected, and the board is in flashing mode. I've attached images of the device manager and COM settings on Uniflash as a reference. I also noticed that there's a forum post that has the same issue, but I decided to make my own since it didn't get resolved. I've followed everything that this poster has done as well. Just hoping to get this solved soon.
Thanks