Other Parts Discussed in Thread: TMCS1123
Hello,
we are planning to use the TMCS1101 for current sensing on the mains side (European 230V grid), to then read the output on a SELV side.
We have a cut on the PCB, running underneath TMCS1101 to further separate the two sides.
The complete device, including the TMCS1101, is then fully potted in polyurethane resin (for reasons other than electrical insulation, and rather related to the operational environment).
Putting aside package clearance and creepage issues, which are dealt with separately as explained above:
internally to the package, for that particular material used, would the datasheet DTI =60um correspond to reinforced isolation suitable also for 230Vac mains applications?
Many thanks in advance,
Luca