This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] IWRL6432: IWRL6432 compRangeBiasAndRxChanPhase calibration

Part Number: IWRL6432
Other Parts Discussed in Thread: IWRL1432,

Steps for generating the compRangeBiasAndRxChanPhase line for the IWRL6432. Similar steps can be taken for the IWRL1432, just substitute 1432 for 6432 as appropriate.

1. Load the motion and presence demo found at C:\ti\MMWAVE_L_SDK_05_03_00_02\examples\mmw_demo\motion_and_presence_detection\prebuilt_binaries\xwrL64xx (or xwrl14xx for the IWRL1432 device).

2. Set a strong target like corner reflector at the distance of X meter (X less than 50 cm is not recommended) at boresight in a clutter-free environment. A large room or outdoors should be sufficient.

3. Add the following line to the configuration file intended for use. It is important to calibrate with a configuration file whose frequency range is similar to the range used in operation.

measureRangeBiasAndRxChanPhase 1 X D

The first argument "1" is to enable the measurement. The second argument, D, (in meters) is the distance of window around X where the peak will be searched. The purpose of the search window is to allow the test environment from not being overly constrained say because it may not be possible to clear it of all reflectors that may be stronger than the one used for calibration. The window size is recommended to be at least the distance equivalent of a few range bins.

4. Ensure that the configuration file fulfills the following constraints: 

Constraint 1 Major Motion must be enabled

Third argument of sigProcChainCfg must be 1 or 3

sigProcChainCfg 32 2 3 0 0 0 0 15

Constraint 2 Static Clutter Removal must be turned off  clutterRemoval 0
Constraint 3 Phase Modulation Mode must be TDM, not BPM

Fifth Argument of chirpComnCfg must be 1

chirpComnCfg 23 0 0 256 1 65.6 0

Constraint 4

Number of TX antennas must be 2

Number of RX antennas must be 3

channelCfg 7 3 0

An example of the changes needed can be found here in MotionDetectConfiguration.cfg

0066.MotionDetectCalibration.cfg

Use this version of the Industrial Visualizer to get output. Replace the python files in the Industrial Visualizer with those given below or just run the executable standalone.

Python Files :https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/1023/3630.gui_5F00_main.py

import struct
import sys
import serial
import binascii
import time
import numpy as np
import math

import os
import datetime

# Local File Imports
from parseTLVs import *
from gui_common import *

def parseStandardFrame(frameData):
    # Constants for parsing frame header
    headerStruct = 'Q8I'
    frameHeaderLen = struct.calcsize(headerStruct)
    tlvHeaderLength = 8

    # Define the function's output structure and initialize error field to no error
    outputDict = {}
    outputDict['error'] = 0

    # A sum to track the frame packet length for verification for transmission integrity 
    totalLenCheck = 0   

    # Read in frame Header
    try:
        magic, version, totalPacketLen, platform, frameNum, timeCPUCycles, numDetectedObj, numTLVs, subFrameNum = struct.unpack(headerStruct, frameData[:frameHeaderLen])
    except:
        print('Error: Could not read frame header')
        outputDict['error'] = 1

    # Move frameData ptr to start of 1st TLV   
    frameData = frameData[frameHeaderLen:]
    totalLenCheck += frameHeaderLen

    # Save frame number to output
    outputDict['frameNum'] = frameNum

    # Initialize the point cloud struct since it is modified by multiple TLV's
    # Each point has the following: X, Y, Z, Doppler, SNR, Noise, Track index
    outputDict['pointCloud'] = np.zeros((numDetectedObj, 7), np.float64)
    # Initialize the track indexes to a value which indicates no track
    outputDict['pointCloud'][:, 6] = 255
    # Find and parse all TLV's
    for i in range(numTLVs):
        try:
            tlvType, tlvLength = tlvHeaderDecode(frameData[:tlvHeaderLength])
            frameData = frameData[tlvHeaderLength:]
            totalLenCheck += tlvHeaderLength
        except:
            print('TLV Header Parsing Failure: Ignored frame due to parsing error')
            outputDict['error'] = 2
            return {}

        # Detected Points
        if (tlvType == MMWDEMO_OUTPUT_MSG_DETECTED_POINTS):
            outputDict['numDetectedPoints'], outputDict['pointCloud'] = parsePointCloudTLV(frameData[:tlvLength], tlvLength, outputDict['pointCloud'])
        # Range Profile
        elif (tlvType == MMWDEMO_OUTPUT_MSG_RANGE_PROFILE):
            outputDict['rangeProfile'] = parseRangeProfileTLV(frameData[:tlvLength])
        # Range Profile
        elif (tlvType == MMWDEMO_OUTPUT_EXT_MSG_RANGE_PROFILE_MAJOR):
            outputDict['rangeProfileMajor'] = parseRangeProfileTLV(frameData[:tlvLength])
        # Range Profile
        elif (tlvType == MMWDEMO_OUTPUT_EXT_MSG_RANGE_PROFILE_MINOR):
            outputDict['rangeProfileMinor'] = parseRangeProfileTLV(frameData[:tlvLength])
        # Noise Profile
        elif (tlvType == MMWDEMO_OUTPUT_MSG_NOISE_PROFILE):
            pass
        # Static Azimuth Heatmap
        elif (tlvType == MMWDEMO_OUTPUT_MSG_AZIMUT_STATIC_HEAT_MAP):
            pass
        # Range Doppler Heatmap
        elif (tlvType == MMWDEMO_OUTPUT_MSG_RANGE_DOPPLER_HEAT_MAP):
            pass
        # Performance Statistics
        elif (tlvType == MMWDEMO_OUTPUT_MSG_STATS):
            pass
        # Side Info
        elif (tlvType == MMWDEMO_OUTPUT_MSG_DETECTED_POINTS_SIDE_INFO):
            outputDict['pointCloud'] = parseSideInfoTLV(frameData[:tlvLength], tlvLength, outputDict['pointCloud'])
         # Azimuth Elevation Static Heatmap
        elif (tlvType == MMWDEMO_OUTPUT_MSG_AZIMUT_ELEVATION_STATIC_HEAT_MAP):
            pass
        # Temperature Statistics
        elif (tlvType == MMWDEMO_OUTPUT_MSG_TEMPERATURE_STATS):
            pass
        # Spherical Points
        elif (tlvType == MMWDEMO_OUTPUT_MSG_SPHERICAL_POINTS):
            outputDict['numDetectedPoints'], outputDict['pointCloud'] = parseSphericalPointCloudTLV(frameData[:tlvLength], tlvLength, outputDict['pointCloud'])
        # Target 3D
        elif (tlvType == MMWDEMO_OUTPUT_MSG_TRACKERPROC_3D_TARGET_LIST or tlvType == MMWDEMO_OUTPUT_EXT_MSG_TARGET_LIST):
            outputDict['numDetectedTracks'], outputDict['trackData'] = parseTrackTLV(frameData[:tlvLength], tlvLength)
        elif (tlvType == MMWDEMO_OUTPUT_MSG_TRACKERPROC_TARGET_HEIGHT):
            outputDict['numDetectedHeights'], outputDict['heightData'] = parseTrackHeightTLV(frameData[:tlvLength], tlvLength)
         # Target index
        elif (tlvType == MMWDEMO_OUTPUT_MSG_TRACKERPROC_TARGET_INDEX or tlvType ==  MMWDEMO_OUTPUT_EXT_MSG_TARGET_INDEX):
            outputDict['trackIndexes'] = parseTargetIndexTLV(frameData[:tlvLength], tlvLength)
         # Capon Compressed Spherical Coordinates
        elif (tlvType == MMWDEMO_OUTPUT_MSG_COMPRESSED_POINTS):
            outputDict['numDetectedPoints'], outputDict['pointCloud'] = parseCompressedSphericalPointCloudTLV(frameData[:tlvLength], tlvLength, outputDict['pointCloud'])
        # Presence Indication
        elif (tlvType == MMWDEMO_OUTPUT_MSG_PRESCENCE_INDICATION):
            pass
        # Occupancy State Machine
        elif (tlvType == MMWDEMO_OUTPUT_MSG_OCCUPANCY_STATE_MACHINE):
            outputDict['occupancy'] = parseOccStateMachTLV(frameData[:tlvLength])
        elif (tlvType == MMWDEMO_OUTPUT_MSG_VITALSIGNS):
            outputDict['vitals'] = parseVitalSignsTLV(frameData[:tlvLength], tlvLength)
        elif(tlvType == MMWDEMO_OUTPUT_EXT_MSG_DETECTED_POINTS):
            outputDict['numDetectedPoints'], outputDict['pointCloud'] = parsePointCloudExtTLV(frameData[:tlvLength], tlvLength, outputDict['pointCloud'])
        elif (tlvType == MMWDEMO_OUTPUT_MSG_GESTURE_FEATURES_6843):
            outputDict['features'] = parseGestureFeaturesTLV(frameData[:tlvLength])
        elif (tlvType == MMWDEMO_OUTPUT_MSG_GESTURE_OUTPUT_PROB_6843):
            outputDict['gestureNeuralNetProb'] = parseGestureProbTLV6843(frameData[:tlvLength])
        elif (tlvType == MMWDEMO_OUTPUT_MSG_GESTURE_FEATURES_6432): # 6432 features output 350
            outputDict['gestureFeatures'] = parseGestureFeaturesTLV6432(frameData[:tlvLength])
        elif (tlvType == MMWDEMO_OUTPUT_MSG_GESTURE_CLASSIFIER_6432):
            outputDict['gesture'] = parseGestureClassifierTLV6432(frameData[:tlvLength])
        elif (tlvType == MMWDEMO_OUTPUT_MSG_GESTURE_PRESENCE_x432):
            # outputDict['gesturePresence'] = parseGesturePresenceTLV6432(frameData[:tlvLength])
            pass
        elif (tlvType == MMWDEMO_OUTPUT_MSG_GESTURE_PRESENCE_THRESH_x432):
            pass
        # Performance Statistics
        elif (tlvType == MMWDEMO_OUTPUT_MSG_EXT_STATS):
            outputDict['procTimeData'], outputDict['powerData'], outputDict['tempData'] \
            = parseExtStatsTLV(frameData[:tlvLength], tlvLength)
        # Presence Detection in each zone
        elif(tlvType == MMWDEMO_OUTPUT_EXT_MSG_ENHANCED_PRESENCE_INDICATION):
            outputDict['enhancedPresenceDet'] = parseEnhancedPresenceInfoTLV(frameData[:tlvLength], tlvLength)
        # Probabilities output by the classifier
        elif(tlvType == MMWDEMO_OUTPUT_EXT_MSG_CLASSIFIER_INFO):
            outputDict['classifierOutput'] = parseClassifierTLV(frameData[:tlvLength], tlvLength)
        # Raw data from uDoppler extraction around targets
        elif(tlvType == MMWDEMO_OUTPUT_EXT_MSG_MICRO_DOPPLER_RAW_DATA):
            pass
        # uDoppler features from each target
        elif(tlvType == MMWDEMO_OUTPUT_EXT_MSG_MICRO_DOPPLER_FEATURES):
            pass
        # Surface classification value
        elif(tlvType == MMWDEMO_OUTPUT_MSG_SURFACE_CLASSIFICATION):
            outputDict['surfaceClassificationOutput'] = parseSurfaceClassificationTLV(frameData[:tlvLength])
        elif(tlvType == MMWDEMO_OUTPUT_EXT_MSG_RX_CHAN_COMPENSATION_INFO):
            outputDict['rx_chan_comp'] = parseRXChanCompTLV(frameData[:tlvLength], tlvLength)
        else:
            print ("Warning: invalid TLV type: %d" % (tlvType))

        # Move to next TLV
        frameData = frameData[tlvLength:]
        totalLenCheck += tlvLength
    
    # Pad totalLenCheck to the next largest multiple of 32
    # since the device does this to the totalPacketLen for transmission uniformity
    totalLenCheck = 32 * math.ceil(totalLenCheck / 32)

    # Verify the total packet length to detect transmission error that will cause subsequent frames to dropped
    if (totalLenCheck != totalPacketLen):
        print('Warning: Frame packet length read is not equal to totalPacketLen in frame header. Subsequent frames may be dropped.')
        outputDict['error'] = 3

    return outputDict

# Decode TLV Header
def tlvHeaderDecode(data):
    tlvType, tlvLength = struct.unpack('2I', data)
    return tlvType, tlvLength

import struct
import sys
import serial
import binascii
import time
import numpy as np
import math
import os
import datetime

# Local File Imports
from gui_common import *

# ================================================== Common Helper Functions ==================================================

# Convert 3D Spherical Points to Cartesian
# Assumes sphericalPointCloud is an numpy array with at LEAST 3 dimensions
# Order should be Range, Elevation, Azimuth
def sphericalToCartesianPointCloud(sphericalPointCloud):
    shape = sphericalPointCloud.shape
    cartestianPointCloud = sphericalPointCloud.copy()
    if (shape[1] < 3):
        print('Error: Failed to convert spherical point cloud to cartesian due to numpy array with too few dimensions')
        return sphericalPointCloud

    # Compute X
    # Range * sin (azimuth) * cos (elevation)
    cartestianPointCloud[:,0] = sphericalPointCloud[:,0] * np.sin(sphericalPointCloud[:,1]) * np.cos(sphericalPointCloud[:,2]) 
    # Compute Y
    # Range * cos (azimuth) * cos (elevation)
    cartestianPointCloud[:,1] = sphericalPointCloud[:,0] * np.cos(sphericalPointCloud[:,1]) * np.cos(sphericalPointCloud[:,2]) 
    # Compute Z
    # Range * sin (elevation)
    cartestianPointCloud[:,2] = sphericalPointCloud[:,0] * np.sin(sphericalPointCloud[:,2])
    return cartestianPointCloud


# ================================================== Parsing Function For Individual TLV's ==================================================

# Point Cloud TLV from SDK
def parsePointCloudTLV(tlvData, tlvLength, pointCloud):
    pointStruct = '4f'  # X, Y, Z, and Doppler
    pointStructSize = struct.calcsize(pointStruct)
    numPoints = int(tlvLength/pointStructSize)

    for i in range(numPoints):
        try:
            x, y, z, doppler = struct.unpack(pointStruct, tlvData[:pointStructSize])
        except:
            numPoints = i
            print('Error: Point Cloud TLV Parser Failed')
            break
        tlvData = tlvData[pointStructSize:]
        pointCloud[i,0] = x 
        pointCloud[i,1] = y
        pointCloud[i,2] = z
        pointCloud[i,3] = doppler
    return numPoints, pointCloud


# Point Cloud Ext TLV from SDK for IWRL6432
def parsePointCloudExtTLV(tlvData, tlvLength, pointCloud):
    pUnitStruct = '4f2h' # Units for the 5 results to decompress them
    pointStruct = '4h2B' # x y z doppler snr noise
    pUnitSize = struct.calcsize(pUnitStruct)
    pointSize = struct.calcsize(pointStruct)

    # Parse the decompression factors
    try:
        pUnit = struct.unpack(pUnitStruct, tlvData[:pUnitSize])
    except:
            print('Error: Point Cloud TLV Parser Failed')
            return 0, pointCloud
    # Update data pointer
    tlvData = tlvData[pUnitSize:]

    # Parse each point
    numPoints = int((tlvLength-pUnitSize)/pointSize)
    for i in range(numPoints):
        try:
            x, y, z, doppler, snr, noise = struct.unpack(pointStruct, tlvData[:pointSize])
        except:
            numPoints = i
            print('Error: Point Cloud TLV Parser Failed')
            break
        
        tlvData = tlvData[pointSize:]
        # Decompress values
        pointCloud[i,0] = x * pUnit[0]          # x
        pointCloud[i,1] = y * pUnit[0]          # y
        pointCloud[i,2] = z * pUnit[0]          # z
        pointCloud[i,3] = doppler * pUnit[1]    # Dopper
        pointCloud[i,4] = snr * pUnit[2]        # SNR
        pointCloud[i,5] = noise * pUnit[3]      # Noise
    return numPoints, pointCloud

# Enhanced Presence Detection TLV from SDK
def parseEnhancedPresenceInfoTLV(tlvData, tlvLength):
    pointStruct = '1b'  # While there are technically 2 bits per zone, we need to use at least 1 byte to represent
    pointStructSize = struct.calcsize(pointStruct)
    numZones = (tlvData[0]) # First byte in the TLV is the number of zones, the rest of it is the occupancy data
    zonePresence = [0]
    tlvData = tlvData[1:]
    zoneCount = 0
    while(zoneCount < numZones):
        try:
            idx = math.floor((zoneCount)/4)
            zonePresence.append(tlvData[idx] >> (((zoneCount) * 2) % 8) & 3)
            zoneCount = zoneCount + 1
        except:
            print('Error: Enhanced Presence Detection TLV Parser Failed')
            break
    tlvData = tlvData[pointStructSize:]
    return zonePresence

# Side info TLV from SDK
def parseSideInfoTLV(tlvData, tlvLength, pointCloud):
    pointStruct = '2H'  # Two unsigned shorts: SNR and Noise
    pointStructSize = struct.calcsize(pointStruct)
    numPoints = int(tlvLength/pointStructSize)

    for i in range(numPoints):
        try:
            snr, noise = struct.unpack(pointStruct, tlvData[:pointStructSize])
        except:
            numPoints = i
            print('Error: Side Info TLV Parser Failed')
            break
        tlvData = tlvData[pointStructSize:]
        # SNR and Noise are sent as uint16_t which are measured in 0.1 dB Steps
        pointCloud[i,4] = snr * 0.1
        pointCloud[i,5] = noise * 0.1
    return pointCloud

# Range Profile Parser
# MMWDEMO_OUTPUT_MSG_RANGE_PROFILE
def parseRangeProfileTLV(tlvData):
    rangeProfile = []
    rangeDataStruct = 'I' # Every range bin gets a uint32_t
    rangeDataSize = struct.calcsize(rangeDataStruct)

    numRangeBins = int(len(tlvData)/rangeDataSize)
    for i in range(numRangeBins):
        # Read in single range bin data
        try:
            rangeBinData = struct.unpack(rangeDataStruct, tlvData[:rangeDataSize])
        except:
            print(f'Error: Range Profile TLV Parser Failed To Parse Range Bin Number ${i}')
            break
        rangeProfile.append(rangeBinData[0])

        # Move to next value
        tlvData = tlvData[rangeDataSize:]
    return rangeProfile

# Occupancy state machine TLV from small obstacle detection
def parseOccStateMachTLV(tlvData):
    occStateMachOutput = [False] * 32 # Initialize to 32 empty zones
    occStateMachStruct = 'I' # Single uint32_t which holds 32 booleans
    occStateMachLength = struct.calcsize(occStateMachStruct)
    try:
        occStateMachData = struct.unpack(occStateMachStruct, tlvData[:occStateMachLength])
        for i in range(32):
            # Since the occupied/not occupied flags are individual bits in a uint32, mask out each flag one at a time
            occStateMachOutput[i] = ((occStateMachData[0] & (1 << i)) != 0)
    except Exception as e:
        print('Error: Occupancy State Machine TLV Parser Failed')
        print(e)
        return None
    return occStateMachOutput

# Spherical Point Cloud TLV Parser
# MMWDEMO_OUTPUT_MSG_SPHERICAL_POINTS
def parseSphericalPointCloudTLV(tlvData, tlvLength, pointCloud):
    pointStruct = '4f'  # Range, Azimuth, Elevation, and Doppler
    pointStructSize = struct.calcsize(pointStruct)
    numPoints = int(tlvLength/pointStructSize)

    for i in range(numPoints):
        try:
            rng, azimuth, elevation, doppler = struct.unpack(pointStruct, tlvData[:pointStructSize])
        except:
            numPoints = i
            print('Error: Point Cloud TLV Parser Failed')
            break
        tlvData = tlvData[pointStructSize:]
        pointCloud[i,0] = rng
        pointCloud[i,1] = azimuth
        pointCloud[i,2] = elevation
        pointCloud[i,3] = doppler
    
    # Convert from spherical to cartesian
    pointCloud[:,0:3] = sphericalToCartesianPointCloud(pointCloud[:, 0:3])
    return numPoints, pointCloud

# Point Cloud TLV from Capon Chain
# MMWDEMO_OUTPUT_MSG_COMPRESSED_POINTS
def parseCompressedSphericalPointCloudTLV(tlvData, tlvLength, pointCloud):
    pUnitStruct = '5f' # Units for the 5 results to decompress them
    pointStruct = '2bh2H' # Elevation, Azimuth, Doppler, Range, SNR
    pUnitSize = struct.calcsize(pUnitStruct)
    pointSize = struct.calcsize(pointStruct)

    # Parse the decompression factors
    try:
        pUnit = struct.unpack(pUnitStruct, tlvData[:pUnitSize])
    except:
            print('Error: Point Cloud TLV Parser Failed')
            return 0, pointCloud
    # Update data pointer
    tlvData = tlvData[pUnitSize:]

    # Parse each point
    numPoints = int((tlvLength-pUnitSize)/pointSize)
    for i in range(numPoints):
        try:
            elevation, azimuth, doppler, rng, snr = struct.unpack(pointStruct, tlvData[:pointSize])
        except:
            numPoints = i
            print('Error: Point Cloud TLV Parser Failed')
            break
        
        tlvData = tlvData[pointSize:]
        if (azimuth >= 128):
            print ('Az greater than 127')
            azimuth -= 256
        if (elevation >= 128):
            print ('Elev greater than 127')
            elevation -= 256
        if (doppler >= 32768):
            print ('Doppler greater than 32768')
            doppler -= 65536
        # Decompress values
        pointCloud[i,0] = rng * pUnit[3]          # Range
        pointCloud[i,1] = azimuth * pUnit[1]      # Azimuth
        pointCloud[i,2] = elevation * pUnit[0]    # Elevation
        pointCloud[i,3] = doppler * pUnit[2]      # Doppler
        pointCloud[i,4] = snr * pUnit[4]          # SNR

    # Convert from spherical to cartesian
    pointCloud[:,0:3] = sphericalToCartesianPointCloud(pointCloud[:, 0:3])
    return numPoints, pointCloud


# Decode 3D People Counting Target List TLV
# MMWDEMO_OUTPUT_MSG_TRACKERPROC_3D_TARGET_LIST
#3D Struct format
#uint32_t     tid;     /*! @brief   tracking ID */
#float        posX;    /*! @brief   Detected target X coordinate, in m */
#float        posY;    /*! @brief   Detected target Y coordinate, in m */
#float        posZ;    /*! @brief   Detected target Z coordinate, in m */
#float        velX;    /*! @brief   Detected target X velocity, in m/s */
#float        velY;    /*! @brief   Detected target Y velocity, in m/s */
#float        velZ;    /*! @brief   Detected target Z velocity, in m/s */
#float        accX;    /*! @brief   Detected target X acceleration, in m/s2 */
#float        accY;    /*! @brief   Detected target Y acceleration, in m/s2 */
#float        accZ;    /*! @brief   Detected target Z acceleration, in m/s2 */
#float        ec[16];  /*! @brief   Target Error covarience matrix, [4x4 float], in row major order, range, azimuth, elev, doppler */
#float        g;
#float        confidenceLevel;    /*! @brief   Tracker confidence metric*/
def parseTrackTLV(tlvData, tlvLength):
    targetStruct = 'I27f'
    targetSize = struct.calcsize(targetStruct)
    numDetectedTargets = int(tlvLength/targetSize)
    targets = np.empty((numDetectedTargets,16))
    for i in range(numDetectedTargets):
        try:
            targetData = struct.unpack(targetStruct,tlvData[:targetSize])
        except:
            print('ERROR: Target TLV parsing failed')
            return 0, targets

        targets[i,0] = targetData[0] # Target ID
        targets[i,1] = targetData[1] # X Position
        targets[i,2] = targetData[2] # Y Position
        targets[i,3] = targetData[3] # Z Position
        targets[i,4] = targetData[4] # X Velocity
        targets[i,5] = targetData[5] # Y Velocity
        targets[i,6] = targetData[6] # Z Velocity
        targets[i,7] = targetData[7] # X Acceleration
        targets[i,8] = targetData[8] # Y Acceleration
        targets[i,9] = targetData[9] # Z Acceleration
        targets[i,10] = targetData[26] # G
        targets[i,11] = targetData[27] # Confidence Level
        
        # Throw away EC
        tlvData = tlvData[targetSize:]
    return numDetectedTargets, targets

def parseTrackHeightTLV(tlvData, tlvLength):
    targetStruct = 'I2f' #incoming data is an unsigned integer for TID, followed by 2 floats
    targetSize = struct.calcsize(targetStruct)
    numDetectedHeights = int(tlvLength/targetSize)
    heights = np.empty((numDetectedHeights,3))
    for i in range(numDetectedHeights):
        try:
            targetData = struct.unpack(targetStruct,tlvData[i * targetSize:(i + 1) * targetSize])
        except:
            print('ERROR: Target TLV parsing failed')
            return 0, heights

        heights[i,0] = targetData[0] # Target ID
        heights[i,1] = targetData[1] # maxZ
        heights[i,2] = targetData[2] # minZ

    return numDetectedHeights, heights

# Decode Target Index TLV
def parseTargetIndexTLV(tlvData, tlvLength):
    indexStruct = 'B' # One byte per index
    indexSize = struct.calcsize(indexStruct)
    numIndexes = int(tlvLength/indexSize)
    indexes = np.empty(numIndexes)
    for i in range(numIndexes):
        try:
            index = struct.unpack(indexStruct, tlvData[:indexSize])
        except:
            print('ERROR: Target Index TLV Parsing Failed')
            return indexes
        indexes[i] = int(index[0])
        tlvData = tlvData[indexSize:]
    return indexes

def parseVitalSignsTLV (tlvData, tlvLength):
    vitalsStruct = '2H33f'
    vitalsSize = struct.calcsize(vitalsStruct)
    
    # Initialize struct in case of error
    vitalsOutput = {}
    vitalsOutput ['id'] = 999
    vitalsOutput ['rangeBin'] = 0
    vitalsOutput ['breathDeviation'] = 0
    vitalsOutput ['heartRate'] = 0
    vitalsOutput ['breathRate'] = 0
    vitalsOutput ['heartWaveform'] = []
    vitalsOutput ['breathWaveform'] = []

    # Capture data for active patient
    try:
        vitalsData = struct.unpack(vitalsStruct, tlvData[:vitalsSize])
    except:
        print('ERROR: Vitals TLV Parsing Failed')
        return vitalsOutput
    
    # Parse this patient's data
    vitalsOutput ['id'] = vitalsData[0]
    vitalsOutput ['rangeBin'] = vitalsData[1]
    vitalsOutput ['breathDeviation'] = vitalsData[2]
    vitalsOutput ['heartRate'] = vitalsData[3]
    vitalsOutput ['breathRate'] = vitalsData [4]
    vitalsOutput ['heartWaveform'] = np.asarray(vitalsData[5:20])
    vitalsOutput ['breathWaveform'] = np.asarray(vitalsData[20:35])

    # Advance tlv data pointer to end of this TLV
    tlvData = tlvData[vitalsSize:]
    return vitalsOutput

def parseClassifierTLV(tlvData, tlvLength):
    classifierProbabilitiesStruct = str(NUM_CLASSES_IN_CLASSIFIER) + 'c'
    classifierProbabilitiesSize = struct.calcsize(classifierProbabilitiesStruct)
    numDetectedTargets = int(tlvLength/classifierProbabilitiesSize)
    outputProbabilities = np.empty((numDetectedTargets,NUM_CLASSES_IN_CLASSIFIER))
    for i in range(numDetectedTargets):
        try:
            classifierProbabilities = struct.unpack(classifierProbabilitiesStruct,tlvData[:classifierProbabilitiesSize])
        except:
            print('ERROR: Classifier TLV parsing failed')
            return 0, probabilities
        
        for j in range(NUM_CLASSES_IN_CLASSIFIER):
            outputProbabilities[i,j] = float(ord(classifierProbabilities[j])) / 128
        # Throw away EC
        tlvData = tlvData[classifierProbabilitiesSize:]
    return outputProbabilities

# Extracted features for 6843 Gesture Demo
def parseGestureFeaturesTLV(tlvData):
    featuresStruct = '10f'  
    featuresStructSize = struct.calcsize(featuresStruct)
    gesturefeatures = []

    try:
        wtDoppler, wtDopplerPos, wtDopplerNeg, wtRange, numDetections, wtAzimuthMean, wtElevMean, azDoppCorr, wtAzimuthStd, wtdElevStd = struct.unpack(featuresStruct, tlvData[:featuresStructSize])
        gesturefeatures = [wtDoppler, wtDopplerPos, wtDopplerNeg, wtRange, numDetections, wtAzimuthMean, wtElevMean, azDoppCorr, wtAzimuthStd, wtdElevStd]
    except:
        print('Error: Gesture Features TLV Parser Failed')
        return None

    return gesturefeatures

# Raw ANN Probabilities TLV for 6843 Gesture Demo
def parseGestureProbTLV6843(tlvData):
    probStruct = '10f'
    probStructSize = struct.calcsize(probStruct)

    try:
        annOutputProb = struct.unpack(probStruct, tlvData[:probStructSize])
    except:
        print('Error: ANN Probabilities TLV Parser Failed')
        return None

    return annOutputProb

# 6432 Gesture demo features
def parseGestureFeaturesTLV6432(tlvData):
    featuresStruct = '16f'
    featuresStructSize = struct.calcsize(featuresStruct)
    gestureFeatures = []

    try:
        gestureFeatures = struct.unpack(featuresStruct, tlvData[:featuresStructSize])
    except:
        print('Error: Gesture Features TLV Parser Failed')
        return None
    
    return gestureFeatures

# Detected gesture
def parseGestureClassifierTLV6432(tlvData):
    classifierStruct = '1b'
    classifierStructSize = struct.calcsize(classifierStruct)
    classifier_result = 0

    try:
        classifier_result = struct.unpack(classifierStruct, tlvData[:classifierStructSize])
    except:
        print('Error: Classifier Result TLV Parser Failed')
        return None

    return classifier_result[0]
# Surface Classification
def parseSurfaceClassificationTLV(tlvData):
    classifierStruct = '1f'
    classifierStructSize = struct.calcsize(classifierStruct)
    classifier_result = 0

    try:
        classifier_result = struct.unpack(classifierStruct, tlvData[:classifierStructSize])
    except:
        print('Error: Classifier Result TLV Parser Failed')
        return None

    return classifier_result[0]

# Mode in Gesture/KTO demo 
# def parseGesturePresenceTLV6432(tlvData):
#     presenceStruct = '1b'
#     presenceStructSize = struct.calcsize(presenceStruct)
#     presence_result = 0

#     try:
#         presence_result = struct.unpack(presenceStruct, tlvData[:presenceStructSize])
#         print(presence_result)
#     except:
#         print('Error: Gesture Presence Result TLV Parser Failed')
#         return None

#     return presence_result[0]

def parseExtStatsTLV(tlvData, tlvLength):
    extStatsStruct = '2I8H' # Units for the 5 results to decompress them
    extStatsStructSize = struct.calcsize(extStatsStruct)
    # Parse the decompression factors
    try:
        interFrameProcTime, transmitOutTime, power1v8, power3v3, \
        power1v2, power1v2RF, tempRx, tempTx, tempPM, tempDIG = \
        struct.unpack(extStatsStruct, tlvData[:extStatsStructSize])
    except:
            print('Error: Ext Stats Parser Failed')
            return 0

    tlvData = tlvData[extStatsStructSize:]

    procTimeData = {}
    powerData = {}
    tempData = {}
    # print("IFPT : " + str(interFrameProcTime))

    procTimeData['interFrameProcTime'] = interFrameProcTime
    procTimeData['transmitOutTime'] = transmitOutTime

    powerData['power1v8'] = power1v8
    powerData['power3v3'] = power3v3
    powerData['power1v2'] = power1v2
    powerData['power1v2RF'] = power1v2RF

    tempData['tempRx'] = tempRx
    tempData['tempTx'] = tempTx
    tempData['tempPM'] = tempPM
    tempData['tempDIG'] = tempDIG

    return procTimeData, powerData, tempData


def parseRXChanCompTLV(tlvData, tlvLength):
    compStruct = '13f' # One byte per index
    compSize = struct.calcsize(compStruct)
    coefficients = np.empty(compSize)
    try:
        coefficients = struct.unpack(compStruct, tlvData[:compSize])
    except:
        print('ERROR: RX Channel Comp TLV Parsing Failed')
    # Print results to the terminal output
    print("compRangeBiasAndRxChanPhase", end=" ")
    for i in range(13):
        print(f'{coefficients[i]:0.4f}', end=" ")
    print('\n')

 

Executable : https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/1023/mmWave_5F00_Industrial_5F00_Visualizer_5F00_with_5F00_Calibration.exe