Hi,
I have questions about capacitive sensing :
- First, I would like to use capacitive sensing in order to detect a non-organic object. If this is possible, what kind of object (plastic, wood...?) Can it detect?
Is it realistic or is it mandatory to use a human touch with a capacitive sensor?
- Second question is about the use of an electrode matrix with capacitive sensing (organic / non-organic object).
According to the Texas Guide " capacitive sensing basics", there is a method to create a matrix of capacitance detection.
Does each electrode need to be wired with one capacitive sensor or is there a capacitive sensor that could withstand the information of multiple electrodes at once (with multiplexing technique)?
Thanks
ZA+ HA