Other Parts Discussed in Thread: UNIFLASH, AWR2944
Hello Experts,
1. According to the schematics TRCV STB pin is connected to PMIC and it's by default it's connected to pull up resistor. Do I need to initialize the whole PMIC/SPI sequence to set the STB to low and enable the CAN TRCV? any shortcuts ?
2. I am also trying with SDK CAN external loopback interrupt but I am not sure which image shall I flash to external flash.
I tried multiples but I think neither one of them is signed so the ROM SW doesn't copy the image to RAM to be executed.
BR,
Andrew