Other Parts Discussed in Thread: MMWAVE-STUDIO, MMWAVE-SDK,
- Questions about mmwave-STUDIO
・The TI website states that DAC1000EVM or MMWAVE-DCP-EVM is required as a condition for direct connection to the mmwave-STUDIO mmwave sensor module.
Can mmwave-STUDIO be used without these EVMs?
・Is DAC1000EVM or MMWAVE-DCP-EVM necessary for applications that do not require streaming transmission?
- Questions about mmwave-SDK
・If mmwave-SDK is connected to the cloud demo, will mmwave-SDK be automatically executed?
・Can it be used offline?
- Questions about IWR1443BOOST
・Will external commands be obtained from the SPI line or UART line?
・Will external detection condition settings be obtained from the SPI line or the UART line?
・Is the detection data (distance, etc.) obtained from the UART line?
Thanks with Best Regards
H.Imabayashi