Hi Team,
Currently we are working on the overhead people counting demo using the industrial toolbox 4_9_0 (since it has a GUI for this demo)
I tried to use the multi-profile configuration to support for the longer and shorter ranges.
I have the following questions:
a) As mentioned in the document people counting does not support advanced frame configuration. But does it support the multi-profile configuration as mentioned below?
sensorStop flushCfg dfeDataOutputMode 1 channelCfg 15 7 0 adcCfg 2 1 adcbufCfg -1 0 1 1 1 lowPower 0 0 profileCfg 0 61.2 60.00 17.00 50 328965 0 55.27 1 128 2000.00 2 1 36 profileCfg 1 61.2 60.00 17.00 50 328965 0 50.00 1 96 4000.00 0 0 30 chirpCfg 0 0 0 0 0 0 0 1 chirpCfg 1 1 0 0 0 0 0 2 chirpCfg 2 2 0 0 0 0 0 4 chirpCfg 3 3 1 0 0 0 0 1 chirpCfg 4 4 1 0 0 0 0 2 chirpCfg 5 5 10 0 0 0 4
When I tried using this, the radar hung up after the sensorStart. Can you please comment on this?
b)Then, I tried to change the parameters like the ramp constant, number of ADC samples and the sampling rate to observe some changes in the detection. But this time also the radar hangs up after the sensorStart.
Can you suggest some values for the profile configuration so that some changes can be observed in the detection.?
Thanks team in advance.