Other Parts Discussed in Thread: IWR6843AOP, AWR6843
Hi Teams,
I would like to reduce the frame time from current 200 ms to 100 ms
The statement in the configration file be changed as 100ms but failed on the testing process
If I changed back to 200 ms it works well
My question is how to do for reducing frame time
with program codes better
Working based on,
Platform: Windows 10
Project: In Cabin Detection
Hardware: IWR6843AOP
IDE: CCS 12.3.0
SDK: 3.5.0.4
Tool: Radar toolBox 1.10.00.13
Regards,
Kevin