This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117: Which package will be less susceptible to solder-shift for a temperature sensor?

Part Number: TMP117

The datasheet of the TMP117 states not to solder the pad on the DRV (WSON) package. I was curious about this so I read the TI app note that gives some more information about solder-shift.

I'm a bit worried about the effect of mechanical stress on the device, because our application will cover the sensor with a heat-conductive epoxy in order to bond it to the product housing.

The app note mentioned that solder-shift is unpredictable, but I was wondering if anyone has any insight into the following questions:

  1. Is it possible to know whether the DRV (WSON) package or YBG (DSBGA) package would less susceptible to this mechanical shifting effect, when covered in epoxy?
  2. Would covering the device in epoxy have a similar effect to the solder-shift from soldering the die attached pad (DAP)?

Thank you for any information. I'm not particularly knowledgeable IC die bonding and package design. Being able to achieve 0.1 C without calibration would be excellent. Other than the solder-shift, this device would meet that requirement.