This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMAG5273: B1 Variant Not Responding

Part Number: TMAG5273

I'm working with a customer on the TMAG5273. They have designed their application to accept any one of the 8 variants of this device (4 addresses, 2 sensitivity levels). This is done by scanning all four addresses and then reading the device ID.

The customer just built up a bunch of boards with the B1 variant, but it does not seem to be responding to commands on the appropriate address of 0x22. We can ABA swapped it with both an A1 and A2 variant, which is working fine.

Are there any other differences between the B1 variant and the A1 variant other than the default I2C address that we should be aware of?

The devices were purchased through TI.com and I have the purchasing information for lot tracing if it is needed.

Thanks,

Stuart