Part Number: TMCS1108
Hi,
I am using TMCS1108A1BQDR and I need help in calibration of the sensor.
Unfortunately, the application was unidirectional and i choose Bidirectional but it isn't a big problem
I am getting following output
1: 2.49 to 2.51V for 0A or no Load
2: 2.54V for 1A
and so on, just add 50mV per ampere as the sensitivity of this sensor is 50mV/Amp
Now, I want to know, how i can measure the current in between 0 and 1A because it keeps generating same output voltages until it reach to 1A. It probably the resolution of this sensor and here it might be another wrong choice that i made(but not sure)
Is there a way that i can monitor current in between 1A resolution?
I have to measure the current upto 10A and I am using Arduino UNO for now to read analog signal.
Thanks