This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: How to Control the Radar's Transmitting Antenna

Part Number: IWR6843AOPEVM

I would like to ask how to control the radar board to achieve such a sending sequence, can you give a tutorial on the corresponding operation steps

Best Regards,

Gary

  • Hello Gary,

    So to confirm you want TX2 always on while having TX1 and TX3 alternating between on and off?

    Best Regards,

    Pedrhom

  • Hello Pedrhom,

    Yes, in the first chirp I want to design, TX1 and TX2 transmit at the same time; in the second chirp cycle, TX2 and TX3 transmit at the same time.

    I also want to know how the three antennas TX1, TX2, and TX3 transmit at the same time within a chirp cycle. I hope to get more detailed step-by-step instructions.

    Best Regards,

    Gary

  • Hello Gary,

    You can do this via having multiple chirpCfg lines in your CFG file. An example of where we alternate TX antennas is in our Vital Signs demo, note that the way it is alternating in this demo is not the way you need it, but the implementation method will be the same with different values. The mmWave SDK will have details on breaking down the chirpCfg parameter on what each field corresponds with.

    Best Regards,

    Pedrhom