This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000: ultrasonic transducer control

Part Number: TDC1000
Other Parts Discussed in Thread: TDC7200

Hello,

I have a question. I am using the TDC1000 in combination with the TDC7200 and I am using ultrasonic transducers which i build myself. For the ultrasonic transducers I need pulses with a very high voltage (35V), significantly higher than the output voltage from the TDC1000. Is there any possibility or component with which I can realise that?

Best Regards,

Anna-Lena