In another thread, a Ti rep said, "You can request the TMP117 NIST documentation from this link on the product page. TI does not provide the measurement uncertainty of an individual device, but does provide a warranty for each device."
However, in the TMP117 documentation, it says, " The TMP117 units are 100% tested on a production setup that is NIST traceable and verified with equipment that is calibrated to ISO/IEC 17025 accredited standards."
Want to confirm that every TMP117 unit is verified to meet the accuracy/precision levels listed in the documentation against NIST traceable equipment. In other words, is each TMP117 NIST traceable calibrated, meaning that each TMP117 unit has been confirmed to be accurate to within the specified ranges in the documentation against NIST traceable equipment?